Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Product List
RF Low Frequency RF MicroReader Slide 19

The following will look at the significance of each byte of a simple (Read tag) command (“01 02 08 32 38”). The “01” is the Start Byte indicating the start of a command string. The “02” is the length (from the next byte and up to, but not including, the BCC). The “08” is Command I - “0000 1000” – which is the bit pattern that instructs the reader to perform a single command, not to calculate the BCC checksum and to set Power Burst I. The “32” in the Data Field is the 50 ms Power Burst value (50dec = 32hex) and finally, the “38” is the checksum calculated on all data after the Start Byte.

PTM Published on: 2009-03-16