Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Product List
RF Low Frequency RF MicroReader Slide 14

The Command Field 1 sets up the MicroReader’s mode of operation in bits 0 and 1 defining either performance of a single operation or running continuously. Bit 2 is set if a BCC calculation is desired while bits 3 and 5 define the time of Power Burst I (Typically 50 ms) and indicate if Power Burst II is required. Bit 6 indicates that data is to be passed in the data field with bit 7 set if Command Field 2 is required.

PTM Published on: 2009-03-16