Maker.io main logo

DIY Wireless Freezer Monitor: Local Temp Monitoring with ESPHome

25

2026-06-01 | By Nate_Larson

License: Attribution Temperature Wifi ESP32 XIAO

Introduction

If you’ve ever had a refrigerator or freezer unexpectedly quit on you, you know the panic of discovering an appliance full of spoiled food. While some modern appliances include temperature alarms, they often demand privacy trade-offs or only offer basic audible alerts that require you to be nearby. Existing DIY solutions have their own challenges: wireless sensors struggle to transmit through freezer insulation like a Faraday cage, while hardwired sensors typically mean drilling holes or sealing gaps that compromise your appliance’s integrity.

This project walks through how to build a connected, wireless freezer monitor that makes installation easy, with no permanent modifications to the appliance, no batteries to worry about, and virtually eliminates any air leaks due to sensor cables. Plus, it ties into your personal Home Assistant server, so all your data stays local and yours.

This project assumes you already have a Home Assistant server running with ESPHome installed.

Project parts

Required parts:

Required materials

Required tools:

Step 1

Measure out 18-24 inches of the flat flex cable and cut to length with the scissors.

A DigiKey ruler and flat flex cable on a black surfaceA pair of scissors cutting a flat flex cable 

Step 2

The flat flex cable consists of a substrate with flat conductors on it and an insulating coating over the conductors. When looking at the cable from the end, you should be able to determine which side of the cable the conductors are on, as they will be slightly raised.

Close-up of a flat flex cable

Orient the cable on a sturdy work surface with the conductors on top, and carefully use the edge of a sharp knife, held perpendicular to the conductor, to scrape away about 3/16” of the insulation off both ends of each conductor, as shown in the following images. Don’t try to remove all the insulation in one go; just keep scraping away small amounts until the copper is exposed.

A person scraping the insulation from a flat flex cableA knife and a strip of flat flex cable

Step 3

The DS18B20 requires a 4.7K ohm pull-up resistor on the data line. Connect the resistor between the 3.3V pin and the D10 pin, and position the resistor to lie flat, being careful not to short the leads to the shield or other pins or components on the board. Cut the resistor leads flush with the bottom of the board, but do not solder the resistor yet.

A small black circuit board with white textA close up of a circuit boardA close up of a device

Step 4

Place the XIAO board with the pull-up resistor onto the Flat Flex cable so that the bare portion of the conductors align with the XIAO’s GND, 3.3V, and D10 solder pads, as shown below.

A ESP32 XIAO with a strip of flat flex cable

With everything in place, solder the XIAO to the cable while simultaneously soldering the resistor into place. Solder these connections quickly, with a hot iron, as allowing the heat to creep into the cable can melt the plastic substrate, deforming or damaging the cable. Applying a bit of paste flux before soldering will help you make good solder joints quickly, helping to prevent heat damage to the cable.

An ESP32 XIAO next to a jar of paste flux

Step 5

Prepare the other end of the flat flex cable by applying solder to the exposed copper – again, flux is your friend here.

A close-up of a tinned flat flex cable

Trim the sensor’s cable to an appropriate length for your application (I typically leave about 12 inches). Strip and tin the leads, then match them to the connections so GND connects to GND, 3.3V to VCC, and the data line to pin D10 of the XIAO. Solder everything in place. Using flux and pre-tinning will make the connections clean and reliable, which sets you up for success in the next step: testing!

 

A close-up of a wire

While these connections are not ideal due to not pre-tinning the wires and not using flux, resulting in some melting of the flat cable, it still worked

 

Step 6

Attach the antenna to the XIAO board, and use a USB cable to connect the XIAO to your PC. Navigate to your ESPHome Builder dashboard, click the “New Device” button, and select the “New Device Setup” option.

A screenshot of a device setup

Give your new device a name.

A screenshot of a computer message

Click “Connect” and select the port your XIAO ESP32 is connected to, and wait for the initial firmware upload to complete.

A screenshot of a computer programA screenshot of a computerA screenshot of a computer

Now, click edit to customize the configuration for this device and add the one_wire BUS config. Looking at the XIAO pinout diagram, we can see that pin D10, which we are using for the DS18B20 temperature sensor, is GPIO10.

ESP32-C3 XIAO pinout diagramA screenshot of a computer program

Click “Install” to compile the new firmware and push it wirelessly to your XIAO. When the code finishes uploading, watch the logs in the window to find the address of your sensor, which you will need to copy to add to the configuration. If you get a message that no one_wire devices were found, double-check your connections are correct, and your solder joints are good.

A screenshot of a computer program

Click “Edit” to modify the configuration for your device again, adding the sensor configuration, with the address you found in the logs, and name the sensor as you see fit. I also added a filter so if the temperature doesn’t change by a significant amount, it won’t update the server – this helps reduce the number of unnecessary datapoints the device transmits and the server logs.

A screen shot of a computer program

Click install to compile and flash the updated config and watch the logs to see your temperature data start flowing in. With this, we now have a working sensor, so the next steps will be to get it ready for installation.

A screenshot of a computer program

Step 7

Fold the flat flex cable near where it is soldered to the XIAO board so the cable is parallel to the USB connection, but comes away on the antenna end, as shown here.

A circuit board with a cable

Place the magnet into the corner of a plastic bag (such as the one your DigiKey parts arrived in!) and cut off the corner – this will insulate the magnet from the XIAO board so it doesn’t short any of the contacts.

A magnet in a plastic bagA piece of a plastic bag with a round magnet in it

Cut a 2-inch-long piece of the heat shrink tubing, slide it over the XIAO board so the USB connector is just inside the tubing, then slide the magnet (in its plastic sleeve) into the heat shrink on the bottom side of the XIAO board, and position the antenna so the heat shrink will keep it in place and prevent it from catching on anything.

A magnet wrapped in plastic and a piece of heat shrinkA magnet and PCB in heat shrink tubing

With everything in place, carefully shrink the tubing with a heat gun. I recommend starting at the end with the USB connector to ensure it remains accessible and work your way to the other end of the heat shrink until it is snug around the assembly.

A small electronic device with a plastic wrap around itA small electronic device with a plastic wrap around itA small electronic device with a plastic wrap around it

With this end complete, we need to address the open connections where the sensor cable connects to the flat cable. In a well-ventilated area, coat the connections with some liquid electrical tape and allow it to dry. Once dry, ensure the connections are fully coated and sealed against shorts or moisture intrusion.

A close-up of a black bottleAn electrical wire on a table

Installation

Installing the device is straightforward. The magnet securely holds the board to the outside of your fridge or freezer. At the same time, the thin, flat cable passes through the door seal with virtually no air leakage – a major advantage over traditional wired sensors. Position the sensor probe inside your appliance, then secure it with a small cable tie to keep it in place. Connect the XIAO via a USB cable to a nearby 5V power supply. Within moments, you’ll see live temperature data flowing into Home Assistant. From there, you can set up automations and alerts to notify you if the temperature drifts outside your desired range, giving you peace of mind that your food is staying safely cold.

An electronic device on the side of a refrigeratorA close-up of a cable attached to a refrigeratorA flat flex cable passing through a door sealA close-up of sensor probe attached to a light fixture

Conclusion

You’ve now built a practical, wireless freezer monitoring system that solves the real-world problems that plague DIY cold storage monitoring. No batteries to replace, no holes drilled through your appliance, no reliance on manufacturer cloud services; just clean, local data flowing into Home Assistant on your own terms.

From here, the possibilities expand. Consider adding a second sensor for your refrigerator or other temperature-critical appliances (you can have multiple one-wire sensors on a single GPIO pin!). You could add a door sensor to your build to know if the door was left open, and even integrate the data into more complex automations, like triggering notifications only during specific hours or combining freezer alerts with other home automation routines. The ESPHome platform makes it easy to customize and extend your setup as your needs evolve.

Most importantly, you now have reliable monitoring protecting your food and your peace of mind. That unexpected thaw in the middle of the night? You’ll know about it before the damage occurs. That’s the real win.

Número de parte del fabricante 11050
TEMP SENSOR WTRPRF DS18B20 11050
SparkFun Electronics
9,64 €
Ver más Details
Número de parte del fabricante 113991054
XIAO ESP32C3
Seeed Technology Co., Ltd
4,27 €
Ver más Details
Número de parte del fabricante PSR1635-03
CABLE FLAT FLEX 3COND 0.100"
Parlex USA LLC
8,91 €
Ver más Details
Número de parte del fabricante 8023
MAGNET 0.750"D X 0.187"THICK CYL
Radial Magnets, Inc.
1,97 €
Ver más Details
Número de parte del fabricante Q2-F-RK4-1-11-6IN-10
HEATSHRINK KIT RFL 1" COLOR 10PC
Qualtek
4,28 €
Ver más Details
Número de parte del fabricante 8341-50ML
NO CLEAN FLUX PASTE
MG Chemicals
11,67 €
Ver más Details
Número de parte del fabricante 44142
KNIFE POCKET W/LOCKING BLADE
Klein Tools, Inc.
30,95 €
Ver más Details
Número de parte del fabricante 10326
HEATERIZER XL-3000 HEAT GUN
SparkFun Electronics
21,02 €
Ver más Details
Número de parte del fabricante 335MT-55.GB.H
SMARTCUT SCISSORS, STRAIGHT,5.5"
Ideal-tek S.A.
9,11 €
Ver más Details
Número de parte del fabricante PA1117
TOOL WIRE CUT/STRIPPER 24-10AWG
Tempo Communications
16,05 €
Ver más Details
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.