Maker.io main logo

Bluetooth Low Energy-based RGB LED Strip Color Control From a Web Browse

107

2024-05-13 | By Sheikh Shuhad

License: General Public License Bluetooth / BLE

1. Introduction

This project is about Bluetooth Low Energy-based RGB LED Strip Color Control from a web browser and STM 32. The LED light strip can also be controlled wirelessly via a BLE scanning App using IOS or Android. With the received data, we decide which color of the RGB strip to activate.

You will need two dongles, one connected to the Nucleo board, and one connected to a computer to control from the web browser. The web script is also available on GitHub. When the BleuIO dongle is connected to the Nucleo board's USB port, the STM32 will recognize it and directly start advertising. This allows the other dongle to connect to it.

It will also accept 3 different inputs from the UART:

input result

0 Send ATI (Request device information) command to BlueIO dongle.

1 Manually turn the LED on

2 Manually turn the LED off

We have used an STM32 Nucleo-144 development board with STM32H743ZI MCU (STM32H743ZI micro mbed-enabled Development Nucleo-144 series ARM® Cortex®-M7 MCU 32-Bit Embedded Evaluation Board) and the WS2812, an intelligent control LED light source, for this example.

Connect the LED to the Nucleo Board by connecting: 4-7 VDC to 5VGND to any GNDDIN to PE9

On the Nucleo NUCLEO-H743ZI2:

BLE project with stm32

Note : If you want to use another setup you will have to make sure it support USB Host and beware that the GPIO setup might be different and may need to be reconfigured in the .ioc file.

2. Project requirements

  • Two BleuIO dongles
  • A board with a STM32 Microcontroller with a USB port. (A Nucleo-144 development board: NUCLEO-H743ZI2, is used for this project.
  • To connect the dongle to the Nucleo board a “USB A to Micro USB B”-cable with a USB A female-to-female adapter can be used.)
  • STM32CubeIDE (https://www.st.com/en/development-tools/stm32cubeide.html)
  • WS2812 RGB LED

3. About the Code

The source code is available at https://github.com/smart-sensor-devices-ab/stm32_bleuio_rgb_led_example

This project is based on another STM32 project (https://github.com/smart-sensor-devices-ab/stm32_bleuio_example) with the interface to the WS2812.

The DIN pin will be connected to TIM1 which need to be enabled in to the .ioc file:

BLE project with stm32

Parameter Settings:

BLE project with stm32

DMA for TIM1 will also be enabled:

BLE project with stm32

In main.c we will need to add a callback for TIM PWM Pulse Finished:

Copy Code
void HAL_TIM_PWM_PulseFinishedCallback(TIM_HandleTypeDef *htim)
{
HAL_TIM_PWM_Stop_DMA(&htim1, TIM_CHANNEL_1);
datasentflag=1;
}

In main.c there is also a functions for controlling the LED.

Set_LED() for changing the color of the individual LEDs.

Set_Brightness() for setting the brightness. A brightness value of 0 means the LED is turned off.

WS2812_Send() executes the changes we made to the LED.

Copy Code
void Set_LED (int LEDnum, int Red, int Green, int Blue)
{
LED_Data[LEDnum][0] = LEDnum;
LED_Data[LEDnum][1] = Green;
LED_Data[LEDnum][2] = Red;
LED_Data[LEDnum][3] = Blue;
}

#define PI 3.14159265

void Set_Brightness (int brightness) // 0-45
{
#if USE_BRIGHTNESS

if (brightness > 45) brightness = 45;
for (int i=0; i<MAX_LED; i++)
{
LED_Mod[i][0] = LED_Data[i][0];
for (int j=1; j<4; j++)
{
float angle = 90-brightness; // in degrees
angle = angle*PI / 180; // in rad
LED_Mod[i][j] = (LED_Data[i][j])/(tan(angle));
}
}

#endif

}

void WS2812_Send (void)
{
uint32_t indx=0;
uint32_t color;


for (int i= 0; i<MAX_LED; i++)
{
#if USE_BRIGHTNESS
color = ((LED_Mod[i][1]<<16) | (LED_Mod[i][2]<<8) | (LED_Mod[i][3]));
#else
color = ((LED_Data[i][1]<<16) | (LED_Data[i][2]<<8) | (LED_Data[i][3]));
#endif

for (int i=23; i>=0; i--)
{
if (color&(1<<i))
{
pwmData[indx] = 60; // 2/3 of 90
}

else pwmData[indx] = 30; // 1/3 of 90

indx++;
}

}

for (int i=0; i<50; i++)
{
pwmData[indx] = 0;
indx++;
}

HAL_TIM_PWM_Start_DMA(&htim1, TIM_CHANNEL_1, (uint32_t *)pwmData, indx);
while (!datasentflag){};
datasentflag = 0;
}

We also updated the handleUartInput function so we can have manual control over the LED via the UART.

Copy Code
/**
* @brief Simple uart input handler
* @retval None
*/
void handleUartInput(UARTCommandTypeDef cmd)
{
switch(cmd)
{
case UART_RX_0:
{
// 0
uart_buf_len = sprintf(uart_tx_buf, "\r\n(0 pressed)\r\n");
HAL_UART_Transmit(&huart3, (uint8_t *)uart_tx_buf, uart_buf_len, HAL_MAX_DELAY);
if(isBleuIOReady)
{
writeToDongle((uint8_t*)DONGLE_CMD_ATI);
} else
{
uart_buf_len = sprintf(uart_tx_buf, BLEUIO_NOT_READY_MSG);
HAL_UART_Transmit(&huart3, (uint8_t *)uart_tx_buf, uart_buf_len, HAL_MAX_DELAY);
}
uartStatus = UART_RX_NONE;
break;
}
case UART_RX_1:
{
// 1
uart_buf_len = sprintf(uart_tx_buf, "\r\n(1 pressed LED on!)\r\n");
HAL_UART_Transmit(&huart3, (uint8_t *)uart_tx_buf, uart_buf_len, HAL_MAX_DELAY);
Set_Brightness(40);
WS2812_Send();
uartStatus = UART_RX_NONE;
break;
}
case UART_RX_2:
{
// 2
uart_buf_len = sprintf(uart_tx_buf, "\r\n(2 pressed LED off!)\r\n");
HAL_UART_Transmit(&huart3, (uint8_t *)uart_tx_buf, uart_buf_len, HAL_MAX_DELAY);
Set_Brightness(0);
WS2812_Send();

uartStatus = UART_RX_NONE;
break;
}
case UART_RX_NONE:
{
break;
}
default:
{
uartStatus = UART_RX_NONE;
break;
}
}
}

4. How to setup project

4.1 Downloading the project from GitHub

Get project HERE https://github.com/smart-sensor-devices-ab/stm32_bleuio_rgb_led_example

Either clone the project or download it as a zip file and unzip it, into your STM32CubeIDE workspace.

4.2 Importing as an Existing Project

From STM32CubeIDE choose File>Import…

stm32 ble project

Then choose General>Existing Projects into Workspace then click ‘Next >’stm32 ble project

Make sure you’ve chosen your workspace in ‘Select root directory:’

You should see the project “stm32_bleuio_rgb_led_example”, check it and click ‘Finish’.stm32 ble project

5. Running the example

  • In STMCubeIDE click the hammer icon to build the project.
  • Open the ‘STMicroelectronics STLink Virtual COM Port’ with a serial terminal emulation program like TeraTerm, Putty, or CoolTerm.

Serial port Setup:

Baudrate: 115200

Data Bits: 8

Parity: None

Stop Bits: 1

Flow Control: None

  • Connect the BleuIO Dongle before running the example
  • In STMCubeIDE click the green play button to flash and run it on your board. The first time you click it the ‘Run Configuration’ window will appear. You can just leave it as is and click run.
  • You should be greeted by this welcome message:

Welcome to STM32 BleuIO RGB LED Example!

Press 0 to run the ATI command

Press 1 to manually turn on LED

Press 2 to manually turn off LED

The LED will turn on briefly when starting up.

stm32 ble project

  • Wait until the message: “[BleuIO Dongle Ready]” is shown.
  • The LEDs should now turn off and you can now connect with the other dongle using the script.

You can also use the uart commands (0, 1 or 2):

  • Press 0 to get device information.
  • 1 to turn on LED.
  • 2 to turn off LED.

Dongle response will be printed to UART.

Control the colors from a web browser

Connect the BleuIO dongle to the computer. Run the web script to connect to the other BleuIO dongle on the STM32. The web script is available inside the source file. Now we can control the colors wirelessly.

For this script to work, we need

Create a simple Html file called index.html which will serve as the frontend of the script. This Html file contains some buttons that help connect and read advertised data from the remote dongle, which is connected to stm32.

Copy Code
<!DOCTYPE html>
<html lang="en">
<head>
<meta charset="UTF-8" />
<meta http-equiv="X-UA-Compatible" content="IE=edge" />
<meta name="viewport" content="width=device-width, initial-scale=1.0" />
<link
href="https://cdn.jsdelivr.net/npm/bootstrap@5.1.3/dist/css/bootstrap.min.css"
rel="stylesheet"
integrity="sha384-1BmE4kWBq78iYhFldvKuhfTAU6auU8tT94WrHftjDbrCEXSU1oBoqyl2QvZ6jIW3"
crossorigin="anonymous"
/>
<title>
Bluetooth controlled RGB LED Strip - Control color from web browser
</title>
</head>
<body class="mt-5">
<div class="container mt-5">
<img
src="https://www.bleuio.com/blog/wp-content/themes/bleuio/images/logo.png"
/>
<h1 class="mb-5">
Bluetooth controlled RGB LED Strip - Control color from web browser
</h1>

<div class="row">
<div class="col-md-4 pt-5">
<button class="btn btn-success mb-2" id="connect">Connect</button>
<form method="post" id="sendMsgForm" name="sendMsgForm">
<div class="mb-3">
<label for="msgToSend" class="form-label"
>Select color option</label
>
<select
class="form-select"
aria-label="Default select example"
name="msgToSend"
id="msgToSend"
required
>
<option selected>Open this select menu</option>
<option value="L=0">LED Off</option>
<option value="L=1">LED On</option>
<option value="L=RED">Set LED lights red</option>
<option value="L=GREEN">Set LED lights green</option>
<option value="L=BLUE">Set LED lights blue</option>
<option value="L=RAINBOW">
Set LEDs lights to different colors
</option>
</select>
</div>

<button type="submit" class="btn btn-primary">Submit</button>
</form>
</div>
<div class="col-md-8">
<img
src="https://www.bleuio.com/blog/wp-content/uploads/2022/09/bluetooth-controlled-rgb-led-strip-collor-control.jpg"
/>
</div>
</div>
</div>

<script src="script.js"></script>
</body>
</html>

Create a js file called script.js and include it at the bottom of the Html file. This js file uses the BleuIO js library to write AT commands and communicate with the other dongle.

Copy Code
import * as my_dongle from 'bleuio'
const dongleToConnect='[0]40:48:FD:E5:2F:17'
document.getElementById('connect').addEventListener('click', function(){
my_dongle.at_connect()
document.getElementById("connect").disabled=true;
document.getElementById("sendMsgForm").hidden=false;
})

document.getElementById("sendMsgForm").addEventListener("submit", function(event){
event.preventDefault()


my_dongle.ati().then((data)=>{
//make central if not
if(JSON.stringify(data).includes("Peripheral")){
console.log('peripheral')
my_dongle.at_central().then((x)=>{
console.log('central now')
})
}
})
.then(()=>{
// connect to dongle
my_dongle.at_getconn().then((y)=>{
if(JSON.stringify(y).includes(dongleToConnect)){
console.log('already connected')
}else{
my_dongle.at_gapconnect(dongleToConnect).then(()=>{
console.log('connected successfully')
})
}
})
.then(()=>{
var theVal = document.getElementById('msgToSend').value;
console.log('Message Send '+theVal)
// send command to show data
my_dongle.at_spssend(theVal).then(()=>{
console.log('Message Send '+theVal)
})
})

})
});

The script has a button to connect to COM port on the computer. After connecting to the dongle , we should be able to control the colors of the LED strip.

To connect to the BleuIO dongle on the STM32, make sure the STM32 is powered up and a BleuIO dongle is connected to it.

Get the MAC address

Follow the steps to get the MAC address of the dongle that is connected to STM32

- Open this site https://bleuio.com/web_terminal.html and click connect to dongle.

- Select the appropriate port to connect.

- Once it says connected, type ATI. This will show dongle information and current status.

- If the dongle is on peripheral role, set it to central by typing AT+CENTRAL

- Now do a gap scan by typing AT+GAPSCAN

- Once you see your dongle on the list ,stop the scan by pressing control+c - Copy the ID and paste it into the script (script.js) line #2Run the web script

stm32 ble project

You will need a web bundler. You can use parcel.js

Once parcel js installed, go to the root directory of web script and type “parcel index.html”. This will start your development environment.

ble stm32

Open the script on a browser. For this example we opened http://localhost:1234

You can easily connect to the dongle and update the LED strip.

The web script looks like this

stm32 ble

Número de parte del fabricante SSD005/4-V2B
BLUETOOTH 5 LOW ENERGY USB DONGL
Smart Sensor Devices
27,55 €
Ver más Details
Número de parte del fabricante NUCLEO-H743ZI
NUCLEO-144 STM32H743ZI EVAL BRD
STMicroelectronics
20,47 €
Ver más Details
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.