IC Block

Simple LED Drivers- MAX7219 and MAX7221

Analog Devices / Maxim Integrated

This presentation will cover an alternative to the most common display technology used today, which are LCD panels, as these panels have drawbacks. For instance, in applications where a high level of contrast is required, LEDs are still chosen over LCDs. One of the more common types of LED displays is the seven segment display. This tutorial will discuss ways to drive these displays with the Maxim MAX7219 and MAX7221.

Related Parts

ImagenNúmero de pieza del fabricanteDescripciónCantidad disponiblePrecio
IC DRVR 7 SEGMENT 8 DIGIT 24DIPMAX7219CNG+IC DRVR 7 SEGMENT 8 DIGIT 24DIP1049 - Inmediata$17.93Ver detalles
IC DRVR 7 SEGMNT 8 DIGIT 24SOICMAX7219CWG+IC DRVR 7 SEGMNT 8 DIGIT 24SOIC1837 - Inmediata$15.64Ver detalles
IC DRVR 7 SEGMNT 8 DIGIT 24SOICMAX7219EWG+IC DRVR 7 SEGMNT 8 DIGIT 24SOIC375 - Inmediata$17.07Ver detalles
IC DRVR 7 SEGMENT 8 DIGIT 24DIPMAX7219ENG+IC DRVR 7 SEGMENT 8 DIGIT 24DIP0 - Inmediata$19.61Ver detalles
IC DRVR 7 SEGMNT 8 DIGIT 24SOICMAX7219CWG+TIC DRVR 7 SEGMNT 8 DIGIT 24SOIC2014 - Inmediata$15.60Ver detalles
IC DRVR 7 SEGMNT 8 DIGIT 24SOICMAX7219CWG+TIC DRVR 7 SEGMNT 8 DIGIT 24SOIC2014 - Inmediata$15.60Ver detalles
IC DRVR 7 SEGMENT 8 DIGIT 24DIPMAX7219CNGIC DRVR 7 SEGMENT 8 DIGIT 24DIP0 - Inmediata$4.39Ver detalles
IC DRVR 7 SEGMNT 8 DIGIT 24SOICMAX7219CWGIC DRVR 7 SEGMNT 8 DIGIT 24SOIC0 - Inmediata$4.39Ver detalles
IC DRVR 7 SEGMNT 8 DIGIT 24SOICMAX7219CWG-TIC DRVR 7 SEGMNT 8 DIGIT 24SOIC0 - Inmediata$4.46Ver detalles
IC DRVR 7 SEGMENT 8 DIGIT 24DIPMAX7219ENGIC DRVR 7 SEGMENT 8 DIGIT 24DIP0 - Inmediata$5.70Ver detalles
PTM Published on: 2015-01-07