The Importance of Calibration in Resistive Touch Screen Systems

Por Microchip Technology

Colaboración de DigiKey


This article will cover the following key issues in the important function of calibration in resistive touch screen systems:
  • What is calibration and why is it important?
  • What challenges are associated with calibration?
  • How is calibration typically handled in resistive touch systems?
Resistive touch technology provides designers with a low cost, low risk option to enhance their designs by adding touch sense as the human interface. Although resistive touch applications are now outpaced by projected capacitive, resistive touch technology continues to be a leader in many touch applications because of its low cost, ease of integration, and acceptance of different input methods including stylus and glove. Common applications for resistive touch include mobile communication devices, personal digital assistants (PDA), global positioning Systems (GPS), Touch Screen Monitors, KIOSK, Media Players, Portable Instruments, and Point of Sale (POS) Terminals.

Design engineers want to quickly and easily integrate touch technology into their embedded system designs for reduced cycle time and risk. They want a drop-in touch screen controller that will “just work” without the learning curve required to become a touch expert and write touch code. Most resistive touch screen controllers are simply analog-to-digital convertors that require time and risk for the designer to develop and integrate into their system. Some resistive touch controllers offer this expertise as part of their black box solution on a standalone microcontroller.

One critical element for successful resistive touch integration is a good calibration routine that ensures accurate touch response. Touch accuracy is a basic customer expectation for any good human interface design. For example, a customer does not want to get a cup of coffee if they touched the hot chocolate button. In this article, we’ll explore the importance of calibration in resistive touch sensor designs and how it is achieved.

What is calibration and why is it important?

One of the biggest design challenges with resistive touch solutions is getting accurate touch coordinates mapped to the specific underlying display via the touch screen. This is known as “calibration”.

Most resistive touch systems require a calibration step as one of the first steps in integration. Calibration of the touch sensor to the display is necessary because it is next to impossible to perfectly align the touch sensor’s coordinates to the underlying display. “Alignment” is a term used to describe the process of scaling and aligning the sensors’ anomalies to the display (Figure 1).

Comparison of non-aligned and aligned sensors

Figure 1: Comparison of non-aligned and aligned sensors.

Calibration can address the concern of touch sensor orientation during manufacturing. Consistent performance of the touch sensor is expected across different product platforms. However, many different pin-outs are associated with touch sensors and can be confusing when trying to produce different system platforms that may use touch screens of varying size or possibly even touch screens from different manufacturers. The different pin configurations of sensors can greatly affect the native operation of the touch controller.

In a scenario of developing and manufacturing two different product platforms, the platforms may use two different brands of touch sensors. Sensor manufacturer A uses one pin configuration, while sensor manufacturer B has the left and right sides switched on the pin configuration of the sensor’s tail. Both manufacturer A and B have great linearity specifications, and are highly responsive. However, manufacturer A has the origin (0,0) designated as the upper-left corner and manufacturer B has designated the upper-right corner as its origin. Calibration is critical to seamlessly re-map the orientation of the origin, allowing for consistently performing products regardless of the sensor’s pin configuration.

This also becomes an issue should the system’s touch sensor need replacement during its lifetime. If a particular manufacturer’s sensor may no longer be available, a second-source sensor may have to be used instead. This new sensor may not have the same orientation as the previous one, so the calibration must be able to correct any anomalies.

Proper calibration of the touch screen to the display is important for touch accuracy. The user wants the system to respond according to the button they pressed and not to the one next to it. Some sensors are less linear than others. Five-wire sensors have an inherent non-linear edge. While activating along the edge, the native controller response would move the cursor in a bowed line. This bowed edge can cause large inaccuracies, especially on systems with large sensor sizes. A calibration routine must include edge-correction in its algorithms. Most often edge-correction is addressed by using a calibration routine that includes processing controller data as the sensor is activated along this edge. This can be achieved by adding calibration targets that fall along the edge of the sensor. This process is often referred to as a “linearization” since it addresses the inherent bowing of the 5-wire sensor by making the controller’s response linear while activating along the edge (Figure 2).

Comparison of a non-linearized and linearized sensor

Figure 2: Comparison of a non-linearized and linearized sensor.

Advanced resistive touch screen controllers with sophisticated calibration algorithms issue touch reports that correct or modify the sensor orientation and precisely map the reported touch location to the physical dimensions of the underlying display. This allows the designer to easily manage the otherwise problematic issue of proper calibration in a touch sensor system.

Challenges associated with calibration, and how calibration is handled


Calibration can be achieved by the controller or via a software driver. This article will focus on controller-driven calibration for embedded systems applications.

A successful touch sensor system has to compensate for a variety of erroneous or changing inputs. Common challenges to proper calibration in touch systems include mechanical misalignment or changing electrical properties to the touch sensor over time. Accurate calibration is critical to manage this variation and provide accurate coordinates.

Typical calibration methods in the industry include using sample data from several points, which meet basic requirements, to provide basic touch coordinates.

Some resistive touch controllers offer advanced controller-based calibration for design simplicity, and do not require the use of a software driver to establish proper calibration. Controller-based calibration provides an intelligent, accurate method for managing calibration across the spectrum of input variables and design complexities. Controller-driven calibration allows for maximum flexibility in embedded designs.

An advanced resistive touch screen controller will offer the option of either reporting raw touch reports or utilizing calibration information to report pre-processed calibrated touch reports. Typically all that is required for the calibration process is for the operator to sequentially touch a series of targets [crosshairs] presented by the host on the display device. The controller then archives the raw-touch data from each calibration touch point (in EEPROM) and uses that data in normal operation to process “raw” data into “calibrated” data.

Both the host and device must understand the geometry of the underlying matrix. The controller can define the matrix by an inset and a specified number of calibration points. The inset defines the margin on the perimeter of the calibration point matrix. This allows for any physical limitations from the bezel. Interior calibration points are spaced equally between the margins. This is illustrated in the following example (Figure 3).

Example: The INSET is predefined as ‘64’ – interpreted as 64/256 (i.e., 25 percent) of the sensor width or height. This defines the ‘margin’ on the perimeter of the calibration point matrix. Interior calibration points are spaced equally between the margins (e.g., for the 9-point calibration in the illustration, point 2 is halfway between points 1 and 3 for calibration in the illustration).

Example of Calibration Inset Calculation

Figure 3: Example of Calibration Inset Calculation.

Conclusion

Advanced calibration is difficult to achieve without sophisticated algorithms that identify and compensate for the mismatch between the display and the touch sensor, as well as other variables. Some highly developed resistive touch screen controllers have advanced proprietary algorithms that allow for this level of calibration in the controller which greatly facilitates incorporating touch in the design.

Advanced resistive touch screen controller solutions do much of the work for the designer by delivering advanced, filtered touch coordinates with on-chip calibration. Proper calibration, along with these sophisticated capabilities, supports enhanced touch features such as signature capture, drawing, and highly accurate button pressing for easy implementation in a wide variety of embedded system designs. These features allow for optimal human interface design with the lowest design risk in resistive touch solutions.

Getting calibration right is critical to the successful integration and use of a touch sensor system. A good human interface design is intuitive and accurate. This means the user will get the expected response when they interact with the device – they will get their cup of hot chocolate as selected.

Microchip’s mTouch™ AR1100 advanced resistive touch screen controllers offer a feature-rich, fully integrated, universal solution including on-chip calibration. The AR1100 touch controllers dynamically adapt to the various touch screen electrical characteristics such as sensitivity, contact resistance, and capacitance to provide optimal performance with minimal design time. Development kits and software tools are readily available to facilitate the integration of touch technology into embedded system designs. Please check out Microchip’s introductory video, inthe video section of their DigiKey supplier page, addressing mTouch AR1100 advanced resistive touch screen controllers.

Note: mTouch is a trademark of Microchip Technology Inc. in the U.S.A., and other countries. All other trademarks mentioned herein are the property of their respective companies.
 
DigiKey logo

Descargo de responsabilidad: Las opiniones, creencias y puntos de vista expresados por los autores o participantes del foro de este sitio web no reflejan necesariamente las opiniones, las creencias y los puntos de vista de DigiKey o de las políticas oficiales de DigiKey.

Información sobre el autor

Microchip Technology

Información sobre la editorial

DigiKey

DigiKey, con sede en Thief River Falls, Minnesota, es un proveedor global de servicios completos de prototipo y diseño, así como de volúmenes de producción de componentes electrónicos que ofrece más de tres millones de productos de más de 750 fabricantes de marcas de calidad en DigiKey.