Making Legacy Automation Part of the Smart Manufacturing Revolution

Por European Editors

Colaboración de Editores europeos de DigiKey

The Industrial Internet of Things (IIoT) is a critical enabler for smart manufacturing, or Industry 4.0 (the fourth industrial revolution), combining automation with big data to increase productivity, reduce waste and energy consumption, and enhance factory flexibility.

Smart manufacturing and the IIoT can empower companies to improve key performance indicators like productivity, equipment uptime and product quality. Companies may be keen to take advantage of the opportunities that are available, but less certain about how to make the change without incurring unacceptable disruption or wasting their investment in existing equipment. The machinery currently in place can represent a significant capital commitment and owners may not be ready to engage in wholesale replacement, or an upgrade project that may involve reprogramming controllers such as PLCs. PLC programs can be complex, and even if enough is known about the current program for successful modification to be possible, the PLC itself may not have enough additional resources available to support the extra functionality.

Adding Smart to existing facilities

To address these concerns, some organizations have explored approaches to introducing web connectivity as an add-on to an existing installation. This can help to lower the cost of entry to smart manufacturing, especially in cases where the installed equipment may contain large numbers of sensors that are used for basic process control. Although rich data may be collected, the lack of external connectivity prevents the organization from realizing its full value.

The Industrial Internet Consortium (IIC) has published the Smart Manufacturing Connectivity Testbed, which proposes a solution for extracting data that normally flows through an I/O module to the PLC. This testbed replaces conventional I/O modules with a gateway that sends the data to an IT system through an additional communication channel using the industry-standard OPC Unified Architecture protocol. By using open standards for communication and a common device model, the IIC proposal enables users to configure and manipulate the sensors via the IT system.

Connect to a machine, connect to the internet

The Panasonic FP7 dual-role PLC has been designed to enable companies to introduce IoT functionality as an add-on to an existing automation system. The controller is equipped to deal with any protocol such as Ethernet/IP, Modbus (RTU and TCP), Profibus and others, allowing it to collect information from an already installed PLC (Figure 1).

Image of Panasonic FP7 dual-role PLC controller

Figure 1: The dual-role controller can collect information from an existing PLC and make it accessible remotely and securely.

A built-in web server enables users to visualize the data using a browser on an ordinary device such as a mobile or desktop PC. The dashboard can be customized using a PC-based creator tool that allows components such as switches, lamps and meters to be selected and arranged by drag and drop, and set up quickly and easily by selecting properties (Figure 2). The FP7 also supports email alerts that can be used to send status updates, event notifications, or exceptional conditions that require immediate attention.

Image of Panasonic FP7 graphics creation tool

Figure 2: The graphics creation tool helps design a clear dashboard to present the collected data.

By directing data from the existing controller to a device such as a smartphone or PC equipped with a browser (Figure 3), the FP7 provides an easy-to-use and low-cost entry point for manufacturers to explore the power of the IoT to enable smart manufacturing practices. It can be added without major disruption, and can connect to multiple automation controllers such as PLCs or other Ethernet compatible equipment, and display data from up to 16 controllers simultaneously. It can also connect to several PCs at the same time.

Image of data can be accessed using any device equipped with a web browser

Figure 3: The data can be accessed using any device equipped with a web browser.

Collected data can be stored securely and managed on the device, and flexible sharing of the controller’s code and data registers maximizes utilization of the available storage and so saves purchasing additional expensive memory. On the other hand, it is also possible to transfer collected data to other media, such as a PC, or via Secure Sockets Layer (SSL) compatible secure communication with an FTP client or a web server on an external LAN. This allows data such as inspection data from a production line to be accumulated on the server and inspected at any time. The FP7 can also read data back from the external devices.

Companies using this approach to IoT connectivity and browser-based process management can extend their smart manufacturing by using the FP7 to transfer captured data to a Cloud-based analytical application.

As a modular PLC that can be configured with a variety of digital and analogue I/O, the FP7 also allows new sensors to be added to the system to provide more detailed information about the process or equipment being monitored. Other modules include positioning units, high-speed counters, pulse output units and remote I/O. This enables a scalable approach to smart manufacturing, permitting users to experience the power of the IoT at a minimal risk before moving on to develop a customized long-term strategy.

Conclusion

In terms of improved manufacturing productivity and business performance, the advantages of smart manufacturing can be clearly understood. However, implementing smart manufacturing cost-effectively and developing a scalable strategy are difficult challenges that can be further complicated by the technical limitations of legacy equipment. Studies such as the IIC’s connectivity testbed have acknowledged the need to add smart manufacturing capabilities to existing facilities with minimal changes to legacy equipment. A dual-role PLC such as the Panasonic FP7 offers a practical solution for realizing greater value from the data currently unavailable from unconnected automation equipment.

 
DigiKey logo

Descargo de responsabilidad: Las opiniones, creencias y puntos de vista expresados por los autores o participantes del foro de este sitio web no reflejan necesariamente las opiniones, las creencias y los puntos de vista de DigiKey o de las políticas oficiales de DigiKey.

Información sobre el autor

European Editors

Información sobre la editorial

Editores europeos de DigiKey