Thermal - Heat Sinks

Cooling devices that work by absorbing heat from an object and then dissipating that heat into the surrounding air.

Bolt On Bolt On Devices that have an opening through which a screw or bolt is inserted in order to fasten the device on to the objects that requires cooling.
View all Bolt On
Clip Clip Devices that require the use of a flexible fastener to hold them on the objects that require cooling.
View all Clip
Press Fit, Push Pin Press Fit, Push Pin Devices that are designed to be mounted to objects they are designed to cool by being pressed over the top of that object or being held in place by pins that are pushed through the device and into the board.
View all Press Fit, Push Pin
Surface Mount Surface Mount Devices that are designed to be mounted to pads located on the top of a printed circuit board. These devices sit over the top of other objects that have been mounted to pads on the board.
View all Surface Mount
Thermal Tape, Adhesive Thermal Tape, Adhesive Devices that require the use of a thermally conductive tape or adhesive to hold them on the objects that require cooling.
View all Thermal Tape, Adhesive
Threaded Coupling Threaded Coupling Devices that consist of two pieces threaded together around the device that requires cooling.
View all Threaded Coupling